HELPDESK
Direct Order
  • SALE%
  • Business Customers
  • Service
  • New Products
  • Helpdesk

Need advice? Mon-Thu, 8am-4.30pm CET, Fri 8am-2pm CET)

Back to Passive Components
  • Passive Components
  • Potentiometers
Back to Passive Components
Potentiometers
  • Potentiometer Accessories
    • Shaft
  • Rotary Potentiometers
    • ALPS potentiometer
    • Linear trimmer
    • Switched trimpod
  • Slide Potentiometers
  • Trimmers

"Do you need any help?"

Conrad Customer Service
  • 0043 50 90 70 - 2000

Potentiometers

Potentiometer Accessories

Potentiometer Accessories

Potentiometer Accessories
Shaft
Rotary Potentiometers

Rotary Potentiometers

Rotary Potentiometers
Linear trimmer ALPS potentiometer Switched trimpod
Slide Potentiometers

Slide Potentiometers

Slide Potentiometers
Trimmers

Trimmers

Trimmers
  • Potentiometer Accessories Potentiometer Accessories
  • Rotary Potentiometers Rotary Potentiometers
  • Slide Potentiometers Slide Potentiometers
  • Trimmers Trimmers
  • Services
  • Guides & Tutorials
  • Product Tests & Reviews
More services

About potentionmeters

  • What is a potentiometer?

  • What types and types of potentiometers are available?

  • Purchase criteria for potentiometers - what is it all about?

  • Conclusion: How to buy the right potentiometer

  • Our practical tip: When replacing, observe the resistance curve, the angle of rotation and the load capacity

  • FAQ - Frequently asked questions about potentiometers

What is a potentiometer?

Related topics related to the potentiometer area

Potentiometers

Potentiometers are passive components whose electrical resistance can be continuously adjusted by mechanical actuation, in contrast to a fixed resistance. They consist of an electrically insulating carrier on which the actual resistance material is applied and a movable contact for removal , also known as a grinder. Potentiometers always have at least three electrical connections , two for the start and end of the actual resistance track and one for the movable sliding contact.

This results in a fixed resistance on the one hand via the total resistance and a continuously adjustable resistance on the other hand through the mechanical division of the resistance path into variable partial resistances on the other. When a voltage is applied, this results in an adjustable voltage divider with corresponding partial voltages.

Potentiometers are used whenever a manual control is to be implemented. Examples are the speed settings for power tools, volume and sound settings on audio devices, the regulation of an output voltage or the brightness level of the lighting via a dimmer. Another very common application of potentiometers is the internal adjustment of electrical and electronic circuits via the variable resistance value or by the use as a voltage divider.

 

What types and types of potentiometers are available?

Rotary Potentiometers

In mechanical terms, potentiometers are distinguished between rotary and sliding potentiometers. A subset of the rotary potentiometers are the trim potentiometers . They do not have an axis for holding an operating button, but usually have a flat slot , or an adjusting screw . They are actuated ("adjusted") using a small screwdriver.

Some potentiometers, usually rotary potentiometers, have an additional switch integrated in their housing. This switch contact, which is then activated at one of the mechanical end positions, is often used to switch a device on and off, for example.

Multiple potentiometers combine two or more potentiometers in one component . A distinction is made here between a common, i.e. mechanically coupled actuation and a separate setting option with two buttons. Special forms of potentiometers are the so-called motor potentiometers . They can be operated both manually and via their mechanically coupled electric actuator. This also enables remote automation of actuating processes.

Trimmers

The electrical properties of potentiometers are defined by the type of resistance material and its linearity. The resistance materials can be a carbon or metal layer, and conductive plastics and composite materials made of ceramic and metal are also commonly used as resistance. The latter are also known as Cermet potentiometers. Wire potentiometers have a screw-shaped resistor wire wound around the (usually ceramic) insulating body, which enables higher electrical power losses than layer potentiometers.

A distinction is made between potentiometers with a linear resistance characteristic corresponding to the operating range and those with a logarithmic characteristic curve. Logarithmic potentiometers are required if a particularly wide setting range is to be implemented, for example for amplifier circuits for volume controls.

 

Purchasing criteria for potentiometers – what is it all about?

Slide Potentiometers

Trim potentiometers often require a particularly precise setting option in order to be able to carry out adjustments very precisely and to minimize operating deviations as much as possible. Multi-turn potentiometers are also available for this purpose, which allow up to 25 complete rotations instead of the usual 210° to 280° rotation angle.

Multi-standard versions are also available in different grades for rotary potentiometers. With up to 10 rotations, particularly precise settings are possible via the rotary knob.

Sliding potentiometers are always available when fast actuation is desired or the current setting position is to be detected quickly and clearly. Arranged next to each other, they also enable the simultaneous operation of several sliding potentiometers, which is common and necessary for mixing desks with their often numerous slide controls.

 

Conclusion: How to buy the right potentiometer

If a high setting accuracy is required, multi-turn potentiometers and trimmers are particularly suitable. Sliding potentiometers enable rapid actuation and allow the position of the slider to be recognized at a glance. Rotary potentiometers and trimmers with rotation angles of up to 280° are relatively universal for most standard applications , they combine an often sufficient setting accuracy with quick access to the desired setting value.

Multiple potentiometers allow common or separate settings as required. Especially in the audio area in stereo applications, they are convenient for adjusting the volume or recording level both together and separately. Wire potentiometers are robust and also available for higher power losses.

In the area of potentiometer accessories you will find a variety of useful additions such as buttons, attachment material, couplings, trimmer wrenches, axle extensions, joint couplings and more.

 

Our practical tip: When replacing the resistor, observe the rotation angle and load capacity

If a defective potentiometer has to be replaced, always make sure that the resistance characteristic (linear, positive or negative logarithmic) corresponds to the original part. The angle of rotation from stop to stop must also be observed when a scale is attached to the device. Of course, the electrical load capacity must not be lower than that of the potentiometer to be replaced.

 

FAQ – Frequently asked questions about potentiometers

What does the "10 k lin" print on a potentiometer mean?

The numerical value indicates the resistance value in ohms, the letter "k" stands for kiloohm, and "M" for megohm. In this case, for a resistance of 10 kiloohms or 10,000 ohms. If there is no further indication or the labeling "lin" below, this is a linear potentiometer. A "+" or "+ log", on the other hand, stands for a positive logarithmic potentiometer, corresponding to "-" or "- log" for a negative logarithmic characteristic of the resistor.

 
About potentionmeters What is a potentiometer? What types and types of potentiometers are available? Purchase criteria for potentiometers - what is it all about? Conclusion: How to buy the right potentiometer ...
  • Secure Payment
  • Trusted Shop
  • Global Shipping
  • 2 Years Warranty
  • 30 Days Money Back Guarantee
Helpdesk
  • Ordering
  • Global Shipping
  • Payment
  • Return & Warranty
  • Affiliate
  • Technology in focus - automation
About Conrad
  • YOUR SOURCING PLATFORM
  • Company
  • WEEE-Recycling
  • Imprint
  • Terms & Conditions
  • Privacy Policy
  • Conrad Connect
Our Services
  • eProcurement
  • PCB - Service
  • PCB - Software
  • Cable Configuration Service
  • Download Center
Contact
Helpdesk
More contacts
Trusted payments MasterCard VISA PayPal American Express Diners Club
Visit our social websites
Trusted Delivery DHL - Global Shipping UPS - Global Shipping Trusted Shops

2020 © Conrad Electronic International GmbH & CoKG - All rights reserved.

v1.9.3.2 (cfdc8dff6-cwbvm)

Choose your country

Switch between our Conrad shops

  • België
  • Conrad.com
  • Česká republika
  • Danmark
  • Deutschland
  • France
  • Hrvatska
  • Italia
  • Magyarország
  • Nederland
  • Österreich
  • Polska
  • Slovenija
  • Slovensko
  • Sverige
  • Schweiz