"Do you need any help?"
Cable Strippers
This text is machine translated.
About stripping pliers
-
What was a stripping pliers?
-
What are the stripping pliers?
-
What do you need to pay attention to when purchasing wire stripping pliers?
-
Safe working with stripping pliers
-
Additional functions
-
FAQs: The most common questions about stripping pliers
-
Conclusion: This is how you can find the right stripping pliers
What was a stripping pliers?
Wire strippers are special tools that are used to strip cables. Their function enables a controlled separation of the insulation from the electrical conductor, which is mostly made of plastic or rubber. There is therefore no risk that this will be damaged, such as in the case of improper stripping with the knife or side cutter. Various versions of stripping pliers are used today in DIY as well as professional applications. The following is a brief introduction to the most important models.
What are the stripping pliers?

Conventional stripping pliers:
Conventional wire strippers are generally quite simple in their structure and operation: The pliers have a round or V-shaped opening that cannot be completely closed. The cutting tools are adjusted manually to suit the cable average, unless fixed sizes are specified. The cutting and removal of the insulation can then be carried out without any problem.
Automatic cable stripper
Slightly larger and in their construction much more complex than conventional stripping pliers, most automatic stripping pliers can be recognized as professional tools purely optically. Accordingly, the tools in this product category are a little more expensive in comparison, but also allow professional users to work faster and more safely.
What do you need to pay attention to when purchasing wire stripping pliers?
Cable stripper type
- Conventional model
- Automatic model
- Model with additional functions
Processing of stripping pliers
- Use of high-quality materials
- Ergonomic design
- Easy to use
Cable specifications
- Size of cable (minimum and maximum cable cross-section)
- Type of cable (e.g. Single wires, flat cables, coaxial cables)
- Quality of the insulation (e.g. PVC, rubber)
Practical advice
Automatic stripping pliers are increasingly used in the professional sector. Once the insulation thickness is set, the tool automatically adapts to the external diameter of the current conductor. Damage to the conductor is thus excluded. Conclusion: Automatic wire stripping pliers enable a particularly fast and safe working.
Safe working with stripping pliers
All work on electrical equipment requires a high degree of accuracy and care. Therefore, it is strongly advised not to strip the insulation using a knife or side cutter. Instead, suitable tools should be used if necessary: Wire stripping pliers offer safety and precision. Of course, the main focus of the tool used is flawless processing. Thus, safe working is not a problem even over long periods of time. In addition, less experienced users should consult the manufacturer's information on the safe handling of the respective stripping pliers before starting work in order to avoid errors from the outset.
Additional functions
Numerous manufacturers offer versatile stripping pliers with additional functions. Automatic wire strippers in particular often still offer the possibility to replace permanently stressed cutting tools with new replacement knives after some time. Also popular are models with length stop or integrated side cutter. These features are explicitly listed in the product description so that a targeted selection of useful additional functions is possible without any problem.
FAQs: The most common questions about stripping pliers
A stripping pliers for all cases – is this possible?
Depending on the model, stripping pliers differ in terms of application possibilities. Particularly versatile models cover a wide range of potential applications, whereas conventional models often require the use of multiple tools. Of course, this difference is also noticeable in the price.
What was the cost of a stripping pliers?
It is important to distinguish once again between the different product groups: While automatic stripping pliers are suitable for professional use in the upper price segment, conventional stripping pliers are comparatively cheap for occasional use. Some special tools (e.g. for wire stripping pliers for flat cables) can also significantly increase costs.
What are the alternatives to stripping pliers?
Abmantler is also suitable as an alternative to stripping pliers for certain applications. However, these cannot be an equivalent replacement for a well-functioning wire stripper. Cable cutters and side cutters are also not an adequate alternative to stripping pliers for the above mentioned reasons.
Conclusion: This is how you can find the right stripping pliers
In the end, various factors decide which stripping pliers are best suited for which application. To avoid mis-purchasing, it is essential to consider technical specifications regarding the cable. In addition, it is useful to learn about the additional features of the different models in order to be able to work much more efficiently with the ideal tool.
Experience has shown that professional users are more likely to opt for the more expensive automatic models. If the tool is only used sporadically, a conventional stripping pliers is usually sufficient. The wide range of products in the shop includes a variety of stripping pliers and offers the right tool for every budget and application.