Full power – especially when on the road

When out in the field providing repair and maintenance services, you can rely on the best tools to get the job done. With smart companions and digital assistants, you are perfectly equipped to face any challenge.

Testo - Digital installation aids, refrigerant scale and app

testo

The service and maintenance team for cooling systems and heat pumps

Using cooling systems consumes considerable resources, making it all the more important to operate these systems professionally and efficiently. Testo products help to ensure the smooth operation of the system. They reliably handle all of your cooling technology measurement tasks. Plus, they make your work more efficient and convenient than ever before.

Calibrating cooling systems: the 557s, 550s and 550i work wirelessly with the smart probes and the testo smart app to measure pressure temperature and humidity.
Filling cooling systems: the new testo 560i works wirelessly with the intelligent valve, the testo smart app and the installation aids to fill by coolant weight, overheating and under cooling.
Evacuating cooling systems: the testo 552i works wirelessly with the testo smart app to carry out cable-free and tubeless vacuum measurement.
 

Testo Brand Shop

Recommended products

Knipex – Pipe and electrical installation

Knipex

Pipe cutting

KNIPEX cutting tools for working with all types of pipes have several things in common: they have been perfectly developed for the specific type of pipe, make work easier by minimising the amount of strength needed, combine multiple work steps in one tool, and are innovative and flexible to use:
For example, the KNIPEX pipe cutter for composite and plastic pipes can be used to cut (90 25 25 zZ in article creation) aluminium composite and plastic pipes up to 26 mm diameter with up to 60 per cent less effort than with conventional shears. The KNIPEX DP50 stands for cutting and chamfering in one step (Create link to the article name 90 23 01 BK CE 2626377). The perfect sanitary installation helper cuts plastic pipes with a diameter of 32, 40 or 50 mm and wall thicknesses of up to 2.4 mm. The KNIPEX TubiX® XL pipe cutter is the specialist (Create link to the article name 90 31 03 BK, CE 2626380) when it comes to perfectly cutting copper, brass and stainless steel pipes with a wall thickness of up to 2 mm inner diameter of 6 to 76 mm (1/4” - 3”).

 

Knipex Brand Shop

Recommended products

Electrical installation

Maximum precision, the highest safety or simply the perfect equipment for every electrical professional - the KNIPEX product portfolio has all this and more. The VDE tool set from KNIPEX focuses on safety, user benefits and quality. The high-quality basic set for electrical installation work consists of voltage-insulated combination pliers, side cutters and flat round nose pliers. The KNIPEX NexStrip® guarantees enormous time savings because the multitool handles cutting, stripping and crimping. Crimping has become one of the most reliable, versatile and cost-effective joining techniques. The self-adjusting crimping pliers for wire-end ferrules for reliable hexagonal crimping of wire-end ferrules and twin wire-end ferrules with extended capacity enables highly precise and standard-compliant work with outstanding ease of use.

Recommended products

Compact, clever, Wera - The right tool always at hand

Wera

Why do people so often not have the right tool at hand? Because having too many tools and heavy toolboxes often make carrying them around a nuisance. That is why we have made it our mission to design tools and tool sets for as many applications as possible which were still easy to transport. Our solution: Kraftform Kompakt tools and tool sets in textile bags. for example, one handle capable of holding blades with different profiles. Compact and safely stored in lightweight and robust textile bags. Plus, various tool and application sets capable of handling diverse jobs with just one set. Compact boxes and bags replace the unwieldy sheet metal toolboxes of the past, which always needed at least one hand to transport. In addition, a set’s significantly reduced weight makes it far more comfortable to carry than ever before. Compact - Clever - Wera.

 

Wera Brand Shop

Recommended products

Voltcraft - Measurement equipment for customer repair service

VOLTCRAFT

A passion for cutting-edge technology and high quality, for more than 40 years. VOLTCRAFT offers a wide range of professional measurement equipment, power supply and charging technology. Mobile measurement equipment for on-site troubleshooting has to meet demanding standards. Long battery life, clearly readable displays under all lighting conditions along with special features to simplify troubleshooting and shorten repair times. VOLTCRAFT has integrated these practical requirements into the development of mobile measuring equipment to support the trades with their day-to-day work.

 

Voltcraft Brand Shop

Recommended products

Recommended products

         

Tool Kits

 

 

Power Tools

 

 

Torque Wrenches

 

Tool Kits

 

Pliers

 

Torque Wrenches

         
         
         

Stripping Tools

 

 

Specialist Tools

 

 

Care Products & Lubricants

 

Stripping Tools

 

Specialist Tools

 

Care Products & Lubricants

         

 

 

We have a wide range of the adhesive’s, adhesive tape and hook and loop fasteners

Discover now ›

 

 

 

Top brands for this field

gedore

HAZET

STAHLWILLE

KNIPEX

NWS

RERENSTEIG

TOOLCRAFT

WERA

WIHA

Bernstein

WELLER

VOLTCRAFT

3M

UVEX

Puma

ALBATROS

SONGEN

KCL