Drone License Guide: Pilot Registration and EU Competency Proof A1/A3
Aktualisiert: 23.06.2022 | Lesedauer: 2 Minuten
This text is machine translated.
The new EU drone regulation has caused unease among many model aircraft enthusiasts who enjoy flying with copters. However, the issue is half as wild as it may seem at first glance.
This is because the extensive regulation, which has been in force since January 1, 2021, must cover all areas of unmanned aviation.
For people who just want to fly their drone outdoors and have fun, we have summarized the most important facts in a nutshell.
Pilot registration
Officially, the pilot registration is called "UAS operator registration". However, it is only required if the drone is equipped with a camera or if a drone without a camera weighs 250 g or more. Registration is carried out online at the Federal Aviation Office (LBA) and can be completed in a few minutes with just a few clicks. You will then receive a registration number (eID number), which must be affixed to the model.
EU certificate of competence (colloquially known as a small drone driver's license)
If the drone you are using weighs 250 g or more, you will need a certificate of competence in addition to registration. For private individuals who only fly their drones for fun, the A1/A3 certificate of competence is essential. This certificate can also be obtained from the Federal Aviation Office. Both the exam preparation and the exam can be carried out easily and quickly online for a fee of currently 25 euros.
Requirements for the use of current copters
| Model | UAS operator registration | Proof of competence A1/A3 | Liability insurance |
|---|---|---|---|
| DJI Mini | X | -- | X |
| DJI Air | X | X | X |
| DJI Mavic | X | X | X |
| DJI Racecopter | X | X | X |
| Revell Go! Video Pro | X | -- | X |
Explanation of the table: (X) = required; (--) not required.
EU drone regulation explained simply
However, according to the EU Drone Regulation, there is more than just operator registration and the EU A1/A3 certificate of competence. There are also other weight classes and different deployment scenarios. These then also require further-reaching competencies and other certificates, such as the EU Remote Pilot Certificate A2 (large drone license). We have compiled all the important information about the EU drone regulation for you on our information page on the EU drone regulation.