The Intel® Evo™ platform: Optimized for business applications
Published: 09.10.2024 | Reading time: 13 minutes
This text is machine translated.
In the modern business world, performance, reliability and efficiency are in demand. As technical possibilities are constantly evolving, companies are faced with the challenge of selecting devices that meet current performance requirements and are as future-proof as possible for years to come.
This is where the Intel® Evo™ platform comes into play. Devices certified for this platform have powerful processors, promise long battery life and offer reliable connectivity. The devices therefore meet the high demands of everyday business life.
How can the Intel® Evo™ platform increase the productivity and efficiency of employees in companies?
What security functions are integrated into the Intel® Evo™ platform and how can they support B2B companies?
In this guide, you will find out what distinguishes the platform in detail and how it can be used effectively in your company.
Intel® Evo™ is a certificate that is only awarded to laptops that fulfill predefined quality characteristics.
The platform developed by Intel® is based on the company's own Project Athena.
In 2019, Intel® worked with IT scientists and industry to analyze how good laptops work as part of an innovation program.
Usage analyses were carried out under real-life conditions in a total of six key areas and the most important features for efficient use were identified.
Users should get the best performance, regardless of whether they are in the office, at home or on the move.
Devices that carry the Intel® Evo™ label today meet strict requirements in the areas of performance, mobility and user experience. This includes fast response times, long battery life and high computing power that is ideal for business applications.
Advantages of the Intel® Evo™ platform for companies
The overriding advantage is obvious: when purchasing, departments know at a glance that selected laptops meet the demanding needs of the company. The label guarantees outstanding performance and reliability, as well as high flexibility and easy integration into existing IT infrastructures.
Let's take a closer look at the requirements of the Intel® Evo™ platform:
Powerful processors and graphics cards
A key feature of the Intel® Evo™ platform is that it is equipped with powerful processors and graphics cards.
At least an 11th generation Intel® Core processor with 8 GB RAM must be installed. Up to the 13th generation, this covers i5, i7 and i9 in detail.
These processors are specially designed to handle demanding tasks such as data analysis, video editing or software development with ease.
The minimum GPU requirement is met by the Iris Xe Graphics.
The graphics card delivers performance that is crucial for visually intensive applications such as 3D modeling or video conferencing in high quality. Alternatively, the Iris Xe MAX graphics card can be installed.
Important:
For the performance of the graphics card to be effective, the display must also be of high quality. As a minimum, the Intel® Evo™ platform sets Full HD at 1,920 x 1,080 pixels. At least a 256 GB NVMe SSD must be installed as storage.
Long battery life and fast charging
The Intel® Evo™ platform sets standards in terms of battery life and energy efficiency. Devices that carry the Evo™ label offer a battery life of at least nine hours. This is tested under realistic conditions and not in the laboratory. The battery therefore lasts for a typical working day, even if users have to work completely mobile on a business trip.
The battery life was calculated for displays in Full HD, not 4K. The maximum runtime decreases with continuous 4K resolution and computing-intensive gaming.
The certification also requires a fast-charging function: after 30 minutes of charging, a notebook must be sufficiently regenerated to work for at least four hours. This function ensures that employees can quickly find a ready-to-use device even during a hectic working day. For companies, this in turn means less downtime and higher productivity.
To ensure that the workflow is uninterrupted, the required performance features also include the “Instand Wake” feature. This means that a laptop in standby requires less than one second to wake up when opened.
Reliable connectivity
Stable connections, even in busy networks, have become essential for workflow. Especially for companies that rely on cloud-based applications or online collaboration platforms, a fast and stable internet connection is of central importance. That's why the certified laptops use Wi-Fi 6 and support the new 6 GHz radio frequency. This reliable connectivity ensures that your employees can work productively at all times without being slowed down by connection problems or slow networks.
The Intel® Evo™ platform also pays attention to reliable hardware interfaces. At least one port is provided for USB-C with Thunderbolt 4. This also provides the Power Delivery function, i.e. the option to turn the notebook into a power source for connected devices.
Acquisition of Evo™-certified devices
Purchasing Evo™-certified devices is easy thanks to the clearly visible label. Companies can see the labels affixed to physical devices or find information about the qualification online in the purchase descriptions.
Every laptop with a certificate scores points in terms of mobile use thanks to its lightweight design and is tailored to business users.
For companies, this means that employees can work with devices that offer high computing power while ensuring stable performance - even with several applications running in parallel.
Important:
When selecting devices, companies should not only look at the PCs, but also consider the specific needs of the employees. Who wants particularly lightweight devices and therefore wants 12-inch devices and which employees prefer their notebook to be available in 15 inches for their day-to-day work? The exact configuration of the available notebooks must be in line with user requirements. This also includes the question of the preferred operating system: The Intel® Evo™ platform supports Windows 11 or Chrome OS.
Integration into existing company infrastructures
Planning and preparation are required for successful integration. IT teams should ensure that the new devices are compatible with existing systems and software solutions after adjusting the network configuration. Thanks to USB-C with Thunderbolt 4 and Wi-Fi 6, this is usually easy for a wide range of networks and peripherals.
Security guidelines can also be checked. The Evo™ certification stipulates that all devices must work with biometric recognition for IT security reasons. Identification via camera and facial recognition as well as via a sensor for scanning fingerprints are common. A third method uses a link to a stored smartphone for authentication.
Cloud services are often used to continuously manage the new devices and to link several B2B companies together. Sophisticated integration at this point ensures that employees can take full advantage of the Intel® Evo™ devices without any interruptions to their workflow.
Employee training for optimal use
The introduction of new technology is only successful if employees are able to use it optimally. Therefore, comprehensive employee training is crucial. This training should cover both basic and advanced functions, including optimal use of processor performance, battery management and connectivity features. Companies can use internal training programs or external training providers to ensure that employees can use the new devices efficiently and productively.
Checking whether a laptop belongs to the Intel® Evo™ platform is a pragmatic step for companies. Notebook providers such as Lenovo, Samsung, Dell and ASUS qualify their best devices for the platform, making it easier for prospective customers to make a purchase decision.
In addition to the high performance and flexibility of the laptops, companies benefit from simple integration into existing infrastructures and efficient use by well-trained employees. With powerful processors, long battery life and reliable connectivity, Evo™-certified devices are ideally suited for business applications. They increase productivity in the long term and contribute to a company's competitiveness.